Measurement & Verification Projects
    The Energy Baseline Identification Measurement & Verification Projects and Reports aim to facilitate energy conservation efforts through accurate baseline calculation, regression analysis, and measurement and verification (M&V) projects. This will enable users to establish an energy baseline, correlate actual against baseline consumption, and assess the effectiveness of energy conservation measures. ISO 50001 provides a structured approach to developing an energy policy, setting targets, and using data to make informed decisions about energy use.
Prerequisites
: Baseline Energy Model.Add Project
      Perform the following steps to create an M&V Project:
- Under theM&V Projectstab, clickAdd Project.Add Project

 - TheAdd Projectpage is displayed. Under theProject Detailspage, provide the following details:
- Name: Provide the Project name. The name is auto-generated; the user can rename it.
 - Methodology: Select a methodology from the four options. Click on the tooltip to know more about the methodology.
- Option A: Retrofit-isolation: Key Parameter Measurement

 - Option B: Retrofit-Isolation: All Parameter Measurement

 - Option C: Whole Facility

 - Option D: (Calibrated Simulation)

 
 - Description: Provide a description for the project. Only 1000 characters are allowed.
 
Project Details
 - ClickNext.
 - User theBaseline Configurationpage, a list of available models from the baseline configurations is displayed. Select a Model from the list, and the data is displayed.Baseline Configuration
NOTE:If a baseline model is already configured with another project, the application displays a warning message as shown in the following image:Model Selection: Error
 - ClickNext.
 - Under theEnergy Conservation Measure (ECM) Detailspage, provide the following details:
- Name: Provide a name (Limit: 35 characters).
 - Start Date: The start date of implemented energy conservation measures. This date is auto-populated, that is, the next date after the Baseline end date.
 - End Date: Select the end date of implemented energy conservation measures.NOTE:The ECM implementation period must not overlap with the baseline period to ensure accurate representation of pre-ECM conditions. If there is an overlap in dates within the Baseline Calculator, Baseline Configuration page, or Reporting page, a pop-up message will prompt the user to adjust the dates.
 - Investment: Provide an investment value. The allowed investment range is from 0.00 to 999,999,999.99 (1 cent less than $1 billion).The currency shown here is configured at the site level. Only two decimals are allowed.
 - Description: Provide a description for the ECM details.
 
Energy Conservation Measure (ECM) Details
 - ClickNext.
 - Under theReporting Periodpage, provide the following details
- Start Date: The start date is auto-populated, that is, the next date after the ECM end date.
 - End Date: Select the end date.
 - Energy Saving Target: Provide the energy-saving target value. The units are selected based on the resource type. Up to 4 decimal places are allowed in this field.
 - Description: Provide a description for the Reporting Period.Reporting Period

 
 - ClickNext.
 - Under theNon-Routine Adjustmentspage, provide the following details:TIP:Non-routine adjustmentsare considered as expected events such as holidays, plant shutdowns, or other non-working periods that significantly alter energy usage patterns.
- If the reporting period does not have any such events, user can skip toPreview.
 
- Name: Provide a name for non-routine adjustments.
 - Start Date: Select the start date within the Reporting period.
 - End Date: Select the end date within the Reporting period.NOTE:While creating another non-routine adjustment, if the time period overlaps with the existing non-routine adjustment, a pop-up message is displayed asking user to adjust the dates.
 - Factor: Select a factor from the dropdown.
 - Value: Provide a non-routine adjustment value.
 
Add Non-Routine Adjustments
 - ClickAdd. The Non-Routine Adjustment is added successfully.User can add multiple non-routine adjustments.Non-Routine Adjustments
NOTE:User can modify these adjustments:- To edit an adjustment, click the [
] icon, change the parameters and click Save. - To delete an adjustment, click the [
] icon. 
 - ClickNext.
 - ThePreviewpage displays the Savings Summary and Actual vs Estimated Consumption chart.Preview

- Saving Summary: The data displayed in the Savings Summary is calculated from the Reporting start date and end date time period.
- Energy Consumption with ECM: The energy consumption reduced due to the efficiency improvements brought by the ECMs.
 - Energy Consumption without ECM: The energy consumption under normal operating conditions without any interventions.
 - Total Savings: The reduction in energy consumption resulting from the implementation of Energy Conservation Measures (ECMs). It is calculated as the difference between the energy consumption (without ECMs) and the post-ECM energy consumption.
 - Payback Period: The time it takes to cover the investment cost from the savings generated by the ECM.
 
 - Actual vs Calculated Baseline Consumption: This graph displays the visual representation between the Actual Baseline Consumption and the Calculated Baseline Consumption.
- Hover the mouse pointer on any data point to view the values.
 - To zoom in, click and drag a particular region in the chart. To reset, clickReset zoom.
 
View Data Points
NOTE:Before saving the M&V project, the user can go back and forth by usingBackandNextaction buttons to re-configure, if required. 
 - ClickSave. The Project is created.Project Created
The user can create a maximum of 10 M&V projects per site. After that, theAdd Projectbutton will be disabled. - The M&V projects table displays the following items:
- Name: The Project name. If the data is updating, a blue dot is displayed, and it may take 15 minutes to reconfigure the changes.
 - Configuration Status: The configuration status of a project.
- Complete: The configuration is complete.
 - Draft: Users can save the project as a draft, preserving all entered details up to the point where all mandatory fields have been completed.
 
 - Energy Savings: The reduction in energy consumption resulting from the implementation of Energy Conservation Measures (ECMs)
 - Emission Reduction (tCO2e): The amount of carbon dioxide equivalent (CO2e) emissions that are prevented due to the implementation of Energy Conservation Measures (ECMs).
 - Cost Savings ($): The total saving in terms of money.
 - Savings Progress (%): The percentage of energy savings achieved to date compared to the expected or target savings over a defined period.
 - Baseline Model: The baseline project used to create the project.
 - Last Modified: The last updated time stamp is displayed in the UTC format.
 - Actions:
- View: To view the Savings Summary and Actual vs Estimated Consumption chart of project.
 - Edit: To edit a project. While editing a project, if the details are invalid or mandatory fields are left blank, the user cannot save the project. Update the changes and clickSave.
 - Delete: To delete a selected project. Click the [
] icon on a desired project. The Delete Projectdialog is displayed, clickDelete. - Download Report: To download the M&V Project report (Format: Microsoft Word). In the downloaded report, the user can add additional details (given below) to the report and save it.NOTE:The units displayed in the reports are based on the source unit of meters. Any changes made to the default unit settings will not be reflected in the downloaded report.
- Document revision control
 - Stakeholders and Project Team
 - M&V Requirements and Key Outcomes
 - ECM intents
 - IPMVP Option and Measurement Boundary
 - Meter Specifications
 - Monitoring responsibilities
 - Expected Accuracy
 - Sampling Error Calculation
 - Modelling Uncertainty Calculation
 - Savings Assessment Uncertainty Calculation
 
 
 
 
Provide Feedback