Properties pane
Certain elements contain properties that you can view and change. Select an element that contains properties to display the
Properties
pane by default. If Properties
does not appear, select View > Properties
.To display properties for element: | Select element from: |
|---|---|
Add-On Instruction |
|
Controller, module, or other device | |
Ladder diagram routine |
|
Program |
|
FactoryTalk Smart Object instance |
|
FactoryTalk Smart Object definition |
|
Tag |
|
Task |
|
User-Defined Type |
|
Provide Feedback