Pane bar
Use the Pane Bar icons to toggle the visibility of panes at specific locations in the user interface.
Item | Description |
|---|---|
![]() | Left panes . Toggle the panes on the left side of the user interface. |
![]() | Explorer . Toggle the selected Explorer pane. |
![]() | Right panes . Toggle the panes on the right side of the user interface. |
![]() | Toolbox . Toggle the Toolbox of instructions to add to a ladder diagram and an Add-On Instruction. |
![]() | Properties . Toggle the Properties pane for the selected element. |
![]() | Copilot . Toggle the Copilot pane for the AI assistant. |
Online . Toggle the Online pane to take your controller online. | |
![]() | Bottom panes . Toggle the panes at the bottom of the user interface. |
![]() | Output . Toggle the error, warning, and information messages that appear for the routines and instructions in the project. |
Provide Feedback