Deploy a project to a controller
Prerequisites
To deploy projects to controllers, you use two applications in addition to
FactoryTalk®
Design Studio™
:- FactoryTalk® Remote Access™Manager. The FactoryTalk Remote Access Manager provides a virtual private network (VPN) connection from FactoryTalk Design Studio in the cloud to controllers and devices on the plant floor. You use FactoryTalk Remote Access Manager to configure an endpoint that connects withFactoryTalk Design Studio.
- FactoryTalk Linx, which provides the browser you use to view the endpoint in the plant and browse to controllers and devices connected to it.
You can access FactoryTalk Remote Access Manager on the FactoryTalk Hub. FactoryTalk Linx
appears in the Deploy center.
TIP:
When you deploy a controller application, if there is a
warning or error in any controller to which you are deploying,
Pre-deployment
issues
opens with a list of controllers, statuses, and issues. Controller
statuses include:- Warnings.Recoverable issues that require user approval to automatically resolve the issue during deployment. For example, you could approve automatic clearing a major fault present in the controller or changing the port mode of the controller.
- Errors. Non-recoverable issues that cannot be resolved. The controller application will not be deployed to the target device.
To deploy a project to a controller
IMPORTANT:
When you deploy a project to one or more controllers, all controllers remain in Program mode. The controllers remain in Program mode until you go online with each controller and set the mode to Run. You can go online with one controller at a time.
- Set the physical controller's key switch or toggle switch to REM (Remote). If the mode switch on the physical controller is set to RUN or PROG, you cannot deploy a project to it from FactoryTalk Design Studio.
- On the top toolbar, select
to open the Deploy center. - If paths are not set for the controllers,set the device pathfor each controller. You can type a path or select the path through the driver in the FactoryTalk Linx browser component. To open the FactoryTalk Linx browser, beside the Path, select
and Set controller path. For specific steps to add a VPN driver, see Add a VPN driver. - Select the check boxes for the controllers to which you want to deploy the project.TIP: Before deploying to a 5069 CompactLogix controller, verify that theEtherNet/IP™port configuration in the project matches the target device.
- SelectDeploy. A progress bar indicates the status of the current build and deployment for each controller.
- IfPre-deployment isssuesopens, review the warnings and errors for each controller application to be deployed:
- If only warnings appear, select all the issues to acknowledge that they will be resolved during deployment and then selectNext.
- If it is undesireable to deploy to the target device due to the warnings, you can selectNextwithout selecting all of the displayed issues. If you do not select all issues, the controller application will not deploy to the target device.
- If any error conditions appear, the controller application will not deploy to the target device. SelectNext.
- At the prompt, select the controller you want to go online with when deployment is complete.Noneis a valid selection.If there are errors during deployment, check theTIP: You can be online with only one controller at a time. If you are currently online with a controller and choose to go online with a different controller, you automatically go offline with the current controller and all monitoring tabs are closed.Output panefor messages. Check theOnline panefor controller status and messages.
Provide Feedback