Add Communications Device to Controller

To add a communications device to a controller, follow these steps:
  1. In
    Devices
    explorer, right-click the backplane and select
    Add device...
  2. In the
    Assign devices to
    dialog, under
    Category filter
    , select
    Communication
    .
  3. Select a device from the list, and under
    Devices to assign
    , choose the number of devices to add to the chassis.
    Select a communication device.
  4. Select
    Continue
    .
  5. Under
    Pending to configure
    , enter the device name, Slot number, and Ethernet address.
    Enter communication device information.
  6. Select
    Finish
    to add the device.
The device appears in the
Devices
explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal