FactoryTalk Smart Objects versus Add-on Instructions
FactoryTalk®
Smart Objects expand on the idea of the Add-on Instruction, but they can
encapsulate other smart objects, multiple programs and routines. FactoryTalk® Smart Object | Add-on Instruction |
|---|---|
Allows for logical code segmentation. | Managed as an instruction. |
Can contain multiple programs, objects, and routines. | One routine only. |
Reusable object that can be standalone or inherit from a definition with options
to override and modify instances. | Based on a definition with multiple instances used in a project. |
Provide Feedback