Configure the Safety Input Module Delay Time

  1. In the configuration tree, right-click the safety input module and select Properties.
  2. In the navigation pane, select Points.
  3. Adjust the input delay time as required for your application.
TIP: See the publication for your safety I/O device for input point specifications.
Input Delay Time
Input Delay Time
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal