Safety Element Indicators
You can use both standard (non-safety-related) and safety-related components in the
control system. In an application, you can perform standard automation control from
standard tasks. Safety controllers provide the same functionality as standard
controllers, with the addition of providing a SIL 2 or SIL 3 capable safety task.
FactoryTalk® Design Studio™
provides a distinction between the
standard and safety-related portions of the application via the safety task, safety
programs, safety routines, safety tags, and safety I/O devices.- The category or class label of Safety indicates safety devices.Safety Device Category
- The
icon decorator indicates safety objects.
Safety Icon Decorator - TheGuardmaster®watermark indicates safety routines.Safety Routine Watermark
Provide Feedback