Safety I/O SNN

The SNN that shows in the Overview tab of the Device profile of an assigned safety I/O matches the SNN shown for the backplane of the safety controller (see Safety Controller Profile). An unassigned safety I/O does not have an SNN until you assign it to a safety controller.
Safety Network Number
Here you can copy, paste, or generate a new SNN in either time-based or manual format (see SNN Formats).
When the safety controller is online with a safety I/O device, the Set button is active. When you commission a safety I/O device for the first time (see Commission a Safety System), you must select Set to write the SNN directly into the device.
For more information about the SNN, see Safety Network Number (SNN).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal