Ownership
When the controller is online, the Ownership setting displays the safety controller to
which the safety device is assigned.
One controller owns each safety I/O device in a safety system. Multiple controllers and
multiple safety I/O devices can be used without restrictions in chassis or on networks.
When a controller owns an I/O device, it stores the configuration data that you define
for that device. This configuration controls how the device operates in the system.
From a control standpoint, one controller controls safety output devices. One controller
also owns each safety input device. However, safety input data can be shared (consumed)
by multiple controllers.
Select Reset Ownership to change the current owner of the safety device configuration.
Ownership reset can only happen when the safety controller is online.
IMPORTANT:
You must ensure that an ownership reset does
not cause an unsafe condition.
See and for more information on safety I/O device replacement.
GuardLogix®
5580 and
Compact GuardLogix®
5380 Controllers Safety
Reference Manual, publication 1756-RM012CompactLogix®
5590
Controller User Manual, publication 1756-UM900Provide Feedback