Online Workspace

To go online with a safety controller, from the Online pane, use the Online-Offline toggle Online-offline toggle icon. When the safety controller is online, the online workspace is available for that safety controller.
TIP: When you go online with a safety application,
FactoryTalk® Design Studio
performs a series of checks and validations and displays errors that prevent going online.
To access the online workspace for a safety controller, select the icon from the Safety Controller Profile.
The following safety functions are available only from the online workspace.
For more information about going online and the online workspace, see Deploy and Monitor in the FactoryTalk Design Studio Online Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal