Safety Signature with Safety Changes

When the safety controller has a safety signature (generated in the Safety Signature ID from the Safety Controller Profile),
FactoryTalk® Design Studio
checks if you have made any safety changes to the offline project since the previous deployment
When you make safety changes and the safety controller has a safety signature, a warning shows that requires you to delete the safety signature. You can either acknowledge the warning, deploy the safety application (which deletes the safety signature), then regenerate the safety signature.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal