Use bitwise operators
    Bitwise operators manipulate the bits within a value based on two values.
The following provides an overview of the bitwise operators. 
| For | Use this operator | 
| bitwise and | and | 
| bitwise or | or | 
| bitwise exclusive or | xor | 
| bitwise complement | not | 
This is an example.
| Use this format | Example | |
| For this situation | Use | |
| value1 operator value2 | If input1, input2, and result1 are DINT tags and your specification says: "Calculate the bitwise result of input1 and input2. Store the result in result1." | result1 := input1 AND input2; | 
Provide Feedback