- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Task attributes
This table describes task attributes.
Attribute | Description |
task type | Type of the task: periodic, continuous, or event. |
name | Name of the task. |
Properties | (optional) Properties of the task. |
Scheduled programs | (optional) Ordered list of program names scheduled within this task. |
Provide Feedback