- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Syntax rules
Syntax rules for the
FactoryTalk Design Studio
programming language align with the IEC 61131-3 standard. Follow these basic syntax rules:
- Syntax is case insensitive. For example, the identifiers abcd, ABCD, and aBCd are treated as identical.
- Element names, or identifiers, can contain up to 40 characters.TIP: When you use the Code Editor to change the name of an object, the references to that object are not updated and might be broken.
- All elements appear in the same general format:
[keyword identifying element] <modifiers for element> [element name];
When an element contains content or sets properties, the code format is extended:
[keyword identifying element] <modifiers for element> [element name] {<element content>< properties := property value >}
- Every statement ends in a semicolon. For example:
tag dint myTag ;
- Not every property, setting, or value must be specified in the programming language. If a setting is not specified, then its default value is used.
- If you don’t specify a desc value, its default is an empty string.
- If you don’t specify a value of a tag, the default value is zero. For example:
tag dint myTag;
In the
myTag
example, the value, description, and other parameters are not specified, so their default values are zero (or an empty string for string datatypes).- Multiple statements can exist on the same line when they are separated by a semicolon. For example:
tag dint myTag ; tag dint myOtherTag
- In ladder routines, a semicolon denotes the end of a line or rung.
- You can insert white space characters in the code to make it more readable. White space characters include non-printing characters such as spaces, tabs, and returns. You cannot insert white space characters inside keywords, literals, enumerated values, and identifiers.
- Use double quotes for descriptions (desc). Use single quotes for tag string values.
Provide Feedback