- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Program properties
This table describes program elements.
Element | Description |
---|---|
program_name | The name of the program. |
Description | Information that describes the program. |
tags | Program-scoped tags. These follow the same format as controller-scoped tags. |
routines | Routines within the program. |
Provide Feedback