- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Program parameter connection syntax
This section describes parameter connection syntax.
Parameter connection syntax defines a connection between two program parameters, or between a program parameter and a controller or device tag. Use parameter connections to share data between programs without using controller-scope tags directly in your logic.
Provide Feedback