- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Keywords in syntax
Keywords are specific identifiers used as individual syntactic elements. Keep these guidelines in mind when using keywords:
- Keywords cannot contain embedded spaces.
- The case of characters is not significant in keywords. For example, the keywordsFORandforare syntactically the same.
- Keywords cannot be used for any other purpose; for example, as variable or element names.
- An identifier preceded with a caret ^ can be the same name as an identifier. For example, you could use the identifier ^tag as an element name.
tag dint ^tag := 0;
Provide Feedback