- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
FactoryTalk Design Studio Project Source Code Syntax
The FactoryTalk Design Studio project source code syntax provides the underlying structure for FactoryTalk Design Studio elements, such as programs, routines, tasks, add-on instructions (AOIs), user-defined data types, and smart objects. Use the code editor to view, edit, and create project source code.
Provide Feedback