Supported Fields for the Spaces Table

The following table provides the supported fields for the Spaces table:
Supported Fields for the Spaces Table
Column Name
Column Type
Description
Example
name
varchar
The name of the space.
cdf_industrial_canvas
createdTime
timestamp
The date when the space was created.
2025-09-07T15:50+00Z
lastUpdatedTime
timestamp
The date when the space was last modified.
2025-09-07T15:50+00Z
isGlobal
bool
It determines whether the space is a global space or not.
true
description
varchar
Description of the space
cdf_industrial_canvas space
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal