Supported Fields for the Data Models Table
The following table provides the supported fields for the Data Models table:
Column Name | Column Type | Description | Example |
---|---|---|---|
externalId | varchar | External ID of the data model. | CogniteCoreDM |
name | varchar | The name of the data model. | CogniteCoreDM |
createdTime | timestamp | The date when the data model was created. | 2025-12-04 09:48:11.929 |
lastUpdatedTime | timestamp | The date when the data model was last modified. | 2025-12-09 07:43:11.929 |
space | varchar | The name of the space in which the data model is created. | cdf_industrial_canvas |
description | varchar | Description of the data model. | Cdf Cognite Model |
Provide Feedback