Supported Fields for the Containers Table
The following table provides the supported fields for the Containers table:
Column Name | Column Type | Description | Example |
---|---|---|---|
name | varchar | The name of the container. | CDF_UserPreferences |
externalId | varchar | The External ID of the container. | CDF_UserPreferences |
space | varchar | The name of the space the container belongs to. | CDF_Industrial_Canvas |
usedFor | varchar | Defines the type of instance. | node |
createdTime | timestamp | The date when the container was created. | 2025-06-07T15:50+00Z |
lastUpdatedTime | timestamp | The date when the container was last updated. | 2025-09-07T15:50+00Z |
Provide Feedback