Internationalization Support for FactoryTalk DataMosaix SaaS
FactoryTalk DataMosaix SaaS
supports multiple languages, including English, Spanish, German, Japanese, Portuguese, French, Italian and Korean. This feature enables users to interact with the application in their preferred language, improving usability and comfort.Switch the application language
Perform the following steps to change the language:
- On theManagement Console,Click on the [
] icon, on the top-right corner of the header.
Language Setting - Hover over theLanguageoption. List of available languages can be seen.Change Language
- Choose the language of your choice from the list, and the UI will be displayed in the selected language.If you selectDeutschfrom the language list, the UI will be displayed in German.UI In German Language
NOTE:
- The currently selected language is highlighted in the language dropdown.
- Language setting is user specific, and not tenant/ organization specific.
- These settings do not affect theFactoryTalk Hubor Main DataMosaix pages.
- When translating labels on the user interface (UI), we areintentionally keeping technical terms, product names, feature names, and similar domain-specific terminology in English. This ensures clarity, consistency, and alignment with industry standards, especially for users who are familiar with these terms in their original form.
Provide Feedback