Features
This topic describes activating or deactivating a feature in
FactoryTalk DataMosaix SaaS
using the Features tab. Before you activate or deactivate a feature, consider the following:
IMPORTANT:
Only the Project Admins can activate and deactivate the features in a project.
- By default, the features manageable option on the Features page is inactive. You need to activate them to enable them to be used inFactoryTalk DataMosaix SaaS.
- When a feature is deactivated, it becomes unavailable to all users of the selected project.
To view the Features page, on the Management Console, navigate to the
Manage Access
tab and click the Features
sub-tab.Features

Provide Feedback