Supported Extractor Versions
The following extractors are supported by the configuration UI. Other extractors are supported using the Custom/Other extractor type:
- ODBC Extractor: v 3.0.0 and later
- OPC UA Extractor: v 2.18
- OSI PI Extractor: v 4.1.0
- FactoryTalk Optix Connector: v 1.03.00
- Asset Framework (PI-AF) Extractor: v 1.5.1
Provide Feedback