Edit Asset

You can edit an existing asset by updating the properties of the asset.
  1. On the Management console, select the
    Modeling
    tab.
    By default,
    All Modeling
    tab is selected and the
    Model Listing
    page is displayed with the available assets.
    Model Listing
  2. Select an asset node.
  3. Click the Edit icon.
    The
    Model Item Detail
    page is displayed.
    Model Item Detail screen
  4. Modify the required asset information and click
    Save
    .
    The updated asset is displayed in the asset list.
    NOTE:
    • You can move an asset from one parent node to another parent node by using the drag-drop action.
    • Moving an asset node from one root to another root is not allowed.
    • A parent node cannot be moved to a child node.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal