Delete Asset
This topic provided information about how you can delete an asset node
- On the Management console, select theModelingtab.By default,All Modelingtab is selected and theModel Listingpage is displayed with the available assets.Select Asset for Deletion
- Select an asset node.
- Click the Delete icon.NOTE:Deletion is permanent. Once you confirm deletion, the delete action cannot be undone.TheConfirm Deletiondialog box is displayed.Confirm Asset Deletion
- ClickYes, Deleteto delete the selected asset.The asset and its child asset nodes are deleted upon confirmation.NOTE:If the selected asset has child asset nodes under it, upon your confirmation, all the child asset nodes including the selected asset node are deleted.
Provide Feedback