Recipe Editor

Use
FactoryTalk Batch Recipe Editor
to create and configure master recipes for use in batch automation. A master recipe is a type of recipe that accounts for equipment capabilities and may include process cell-specific information.
The interface contains IEC 61131‑3 sequential function charts to graphically organize recipes into procedures, unit procedures, operations, and phases. Build recipes using either the SFC format or a table-based format.
Procedural levels:
Recipes use the ISA S88.01 Batch Control Standards for configuration and display, which define these levels for the procedural model:
  • Batch control
    : Consists of a sequence of one or more steps (phases) that must be performed in a defined order for a finite period of time to process finite quantities of input material to produce finished product.
  • Procedure
    : The strategy for carrying out a process. In general, it refers to the strategy for making a batch within a process cell. It may refer to a process that does not result in the production of a product.
    Examples:
    Make Product A
    Make Product B
  • Unit Procedure
    : A strategy for carrying out a contiguous process within a unit. It consists of contiguous operations and the algorithm necessary for the initiation, organization, and control of those operations.
    Examples:
    Emulsification
    Dehydrogenation
  • Operation
    : A procedural element defining an independent processing activity consisting of the algorithm necessary for the initiation, organization, and control of phases.
    Examples:
    Filtration
    Reaction
  • Phase
    : The lowest level of the procedural element in the procedural control model. A phase consists of the control steps and the algorithm necessary for the initiation, organization, and control of those steps.
    Examples:
    Agitate
    Heat
The recipe phase is the lowest level within a recipe. The phase provides an interface to basic control. The recipe phase maps directly to the engineered logic on the plant floor. Base an added phase on a phase already defined in the area model using the
FactoryTalk Batch Equipment Editor
. Based on the unit requirements specified in the recipe, a phase in the
FactoryTalk Batch Equipment Editor
maps to a specific phase (an instance of a phase class). This phase is mapped (using tags) to equipment phase defined in the engineered logic.
An operation consists of one or more recipe phases, and it must run within a single unit in the area model. Combine multiple operations into a single unit procedure if each operation runs in the same unit in the area model. Unit procedures combine to create a procedure, the highest recipe level. Procedures can run across multiple units, allowing for unit-to-unit transfers.
FTB_RE_Recipe Levels
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal