General troubleshooting errors
This section outlines errors that may occur while installing and running
FactoryTalk Batch
and possible solutions.Error: Automatic repair of batch component installation fails
Possible cause | Solution |
---|---|
This may occur if one or more folders were moved in Windows explorer. For example, if the Schema folder gets moved from its original directory, the installation package starts up automatically and tries to repair the problem. This may clear out the Model and Server keys in the registry, which will prevent the batch client editors from finding the Network Model. | Completely uninstall the application and then reinstall it. |
Error:
FactoryTalk Batch
Server does not startPossible cause | Solution |
---|---|
Journal path has not been defined in FactoryTalk Batch Server options. | Modify the FactoryTalk Batch Server options to include a valid Primary Journal path. Verify that the
Secondary Journal path, if defined, is valid. |
Restart path has not been defined in FactoryTalk Batch Server options. | Modify the FactoryTalk Batch Server options to include a valid Primary Restart path. Verify that the
Secondary Restart path, if defined, is valid. |
The FactoryTalk Batch Server is always installed with the default user and password. | Verify that the FactoryTalk Batch Server service user account is correct.
|
Error:
FactoryTalk Batch
Server runs for a specific period of time and then stops, and consistently stops at the
same two-hour intervalPossible cause | Solution |
---|---|
The FactoryTalk Batch Server did not read the product license successfully on startup, and demo mode
was selected by the user to start the FactoryTalk Batch Server service. | Check the FactoryTalk Batch Activation Server and make sure there is a working FactoryTalk Batch server license. You can also check the batchsvr.log file to determine how the
batch server is starting (demo mode or license mode) and change to license mode. |
Error:
FactoryTalk Batch
Service Manager does not display the FactoryTalk Batch
Server or FactoryTalk Event Archiver
Possible cause | Solution |
---|---|
The computer where the services are located is not selected. | Click the Select Computer button and select the appropriate computer. |
The FactoryTalk Batch Server, FactoryTalk Event Archiver , and FactoryTalk
e Procedure | To register a service:
|
Error:
FactoryTalk Batch
Service Manager displays the class name (Batch.Server Class) instead of the display name
(Batch Server)Possible cause | Solution |
---|---|
DCOMCNFG configures the FactoryTalk Batch Server service to display the class name of the service instead of the display
name. | When this occurs, the server no longer supports its COM interface and must be
reinstalled. |
Error: The text in
FactoryTalk Batch
dialog boxes does not display properlyPossible cause | Solution |
---|---|
FactoryTalk Batch does not support the use of large system fonts. | In the Display Properties dialog box, change the default system font size to Small Fonts . |
Error: Unable to locate files. The Recipe directory file could not be found
Possible cause | Solution |
---|---|
The server options for the FactoryTalk Batch Server are not configured to point to the folder that contains the
Recipe.dir file. | Configure the server options to point to the folder containing the Recipe.dir file. See Edit the for more information. FactoryTalk Batch server options |
Error: Application Log error
The Application log file is full
is generatedPossible cause | Solution |
---|---|
The Windows Application log is not set for wrapping. | Use the Event Viewer to change the Application Event Log Wrapping setting to Overwrite Events as Needed :
|
Error: Recipes not visible from
FactoryTalk Batch
View Select a Recipe dialog boxPossible cause | Solution |
---|---|
The Release Recipe to Production check box is not selected in the recipe header data. | For each recipe that should appear in the Select a Recipe dialog box, ensure that the Release Recipe to Production check box is selected. This can be done by selecting the Header Data menu option from the Recipe Editor Recipe menu for the recipe and selecting the Release Recipe to Production check box. |
If recipe approvals are enabled, the Release Recipe to Production step is not approved. | For each recipe that should appear in the Select a Recipe dialog box, ensure that the Release Recipe to Production step is approved. This can be done by signing off on the Release Recipe to Production approval step as part of the approval process defined in the area model for the recipe. |
Error: List of available SQL server databases not displayed in the Server Options or Database Selection dialog box
Possible cause | Solution |
---|---|
When the browse button for SQL server databases is clicked, no databases are displayed in the Database Selection dialog box. | Install the SQL Server Client Tools Connectivity option. Do a custom install of SQL server to install the SQL Server Client Tools Connectivity option. Or just type in the database name. |
Error: Event Journal files are not being created
Possible cause | Solution |
---|---|
If the Primary Journals directory is located on a computer other than the server computer, or not within the BATCHCTL share, and that computer becomes inaccessible, the server continues executing batches but is unable to create event journals for those batches. You will not receive a notification of the problem. | The primary journal directory must be located on the FactoryTalk Batch Server computer in the BATCHCTL share.To mitigate risk of an event journal loss in your system, it is recommended that
a secondary event journal path be established to a local and separate physical
drive on the FactoryTalk Batch Server node, or to a location for networked storage. |
Provide Feedback