COM-related exception errors
General COM-related system or program errors can occur for any number of reasons in processing the import or export request. A generic error handling displays the routine that encountered the error and the reason for the error as supplied by the originator (function) of the error.
If this occurs, an error message displays and the import or export does not occur. Examples include:

Provide Feedback