Windows services

The
FactoryTalk Batch
Server,
FactoryTalk Event Archiver
Server, and
FactoryTalk Event Archiver
operate as Windows services. During
FactoryTalk Batch
installation, the user account specified during the installation is assigned to the
Log On As: This Account:
option, found in the (Administrative Tools)
Services
dialog box.
Running as a Windows service allows the
FactoryTalk Batch
Server to run in the absence of an interactive Windows logon. Logging on or logging off Windows during operation does not disrupt the server execution.
Configure the
FactoryTalk Batch
Server to start automatically, giving server control to Windows Services, or control the
FactoryTalk Batch
Server manually using the
FactoryTalk Batch
Service Manager. The Service Manager also controls the type of boot method that the server uses, and runs the server in demo mode.
TIP:
Specifying the boot method or demo mode in the
FactoryTalk Batch
Service Manager does not alter the Batchsvr.ini file and has no effect on the server when automatically starting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal