FactoryTalk Batch Server user account configuration requirements

Create a Windows user account for the
FactoryTalk Batch
Server prior to installing
FactoryTalk Batch
applications. When installing
FactoryTalk Batch
and
FactoryTalk
e
Procedure
applications, you are prompted to enter this user account.
When creating the server user account, the following configuration requirements must be met.
  • The password must be configured to never expire.
    If the password expired, the batch server service would fail to log on.
  • The server user account must never be disabled or deleted.
    If this account is ever disabled or deleted, the batch server service would fail to log on.
  • The domain user account must have a unique name.
    If the server user account is a domain account, remove any local user accounts with the same name.
  • The Server user account or user group must exist on all workgroup computers.
    If you are using a local account and expect that account to have access to resources on other computers in a workgroup environment, you must create accounts with the same name and password on each computer in the workgroup.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal