Batch listing

These tables outline the different components of the report.
Dataset
Stored Procedure
Comment
GetBatchListByDate
spGetBatchListByDate
Gets the Batches executed between two dates
GetRecipeNames
spGetRecipeNamesBYDate
Gets the Recipes used between two dates
GetUnitName
spGetUnitNameByDate
Gets the Units used between two dates
GetProcessCell
spGetProcessCellByDate
Gets the Process Cells used between two dates
Parameter
Where used
Comment
StartTime
All procedures
Start Time
EndTime
All procedures
End Time
SearchWord
spGetBatchListByDate
User Defined Batch Filter
ProcessCell
NA
Process Cell Filter
RecipeName
NA
Recipe Name Filter
UnitName
NA
Unit Name Filter
Object
Data Item
Data Source
Type
Start Time
StartTime
User input
Parameter
End Time
EndTime
User input
Parameter
Table
Dataset
Comment
table1_GetBatchListByDate
GetBatchListByDate
Batch List
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal