Date and Time view parameters
Parameter | Description |
|---|---|
Current device local time | Displays the local time in the power monitor. |
Set... | Opens a dialog box for configuring parameters related to the date and
time functions. |
Set to workstation date and time settings | Copies your PC’s current date and time to the Date and Time
fields. This parameter is disabled when offline. |
Manually set date and time | Sets the date and time in the power monitor to the values in the Date
and Time fields. This parameter is disabled when offline. |
Date | Displays the date in the power monitor. Edit the displayed date to
change it in the power monitor if desired, or select the icon to
activate a calendar popup dialog. This parameter is disabled when offline. |
Time | Displays the time in the power monitor. Edit the displayed time to
change it in the power monitor if desired. This parameter is disabled when offline. |
Provide Feedback