Path specified invalid or device is not responding
Problem communicating with the device. This may occur when the device is not present,
communication to the device is lost, or the network path to the device is not valid.
Select
OK
, then select Refresh Diagnostics
to refresh communication with the
device.Provide Feedback