Electronic keying
Electronic keying reduces the possibility of using the wrong device in a control system.
Electronic keying compares the device defined in the project to the installed device. If
keying fails, a fault occurs.
These attributes are compared:
Attribute | Description |
|---|---|
Vendor | The device manufacturer. |
Device Type | The general type of the device, for example, digital I/O device. |
Product Code | The specific type of device. The Product Code maps to a catalog number. |
Major Revision | A number that represents the functional capabilities of a device. |
Minor Revision | A number that represents behavior changes in the device. |
These
Electronic keying
options are available:Keying Option | Description |
|---|---|
Compatible Module | Lets the installed device accept the key of the device that is defined in the project when the installed device can emulate the defined device. Typically, use Compatible Module to replace a device with another device that has these characteristics:
|
Disable Keying | Indicates that the keying attributes are not considered when attempting to communicate with a device. With Disable Keying , communication can occur with a device other than the type specified in the project.ATTENTION: Use extreme caution when using Disable Keying .
If used incorrectly, this option can lead to personal injury or death, property
damage, or economic loss.We strongly recommend not using Disable Keying .If using Disable Keying , take full responsibility for understanding whether the device being used can fulfill the functional requirements of the application. |
Exact Match | Indicates that all keying attributes must match to establish communication. If any attribute does not match precisely, communication with the device does not occur. |
Carefully consider the implications of each keying option when selecting one.
IMPORTANT:
- Changing Electronic keying parameters online interrupts connections to the device and any devices that are connected through the device. Connections from other controllers can also be broken.
- A loss of data may occur if an I/O connection to a device is interrupted.
Provide Feedback