Device definition dialog box parameters
The
Device definition
dialog box includes these parameters.
TIP:
Some parameters in the
Device definition
dialog box are not
available for all device types.Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Name | Specifies the device name. The name must be IEC_61131 compliant. If an invalid character is entered in this
field or if the name exceeds 40 characters, the software ignores the character. |
Description | Specifies the description for the device. The description must be within 512 characters. If the description exceeds the
maximum length, the software ignores any extra characters. |
Slot | Specify the slot number where the device resides. Only slots between 1 and the
maximum number of I/O devices are valid depending on the platform. When the device is created, the slot number defaults to the first available slot
position. When the controller is changed to one supporting a smaller maximum I/O count, the
current slot value may no longer be valid. |
Series | Specifies the series of the device. |
Revision | Specifies the major and minor revisions of the device. The valid range for minor revision is from 1 through 255. |
Electronic keying | Defines the electronic keying used for the device. Electronic keying compares the
device defined in the project to the installed device. If keying fails, a fault
occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000
Control Systems Application Technique, publication LOGIX-AT001. |
Connection | Sets the Connection Type or the Communication Format. For detailed information on Rack Connection , see Rack Connection. |
Configured By | Displays the entity that configures the device. Valid values include:
The available values depend on the host software. Values that are not supported by
the software are hidden. |
Input Data / Output Data | Select the input or output data type for the device. |
Output Mode | Defines the output mode of the device. |
Counters | Select the counter number for the device. |
Ethernet address | Specifies the IP configuration for the device. Possible options include:
|
Enable Network Address Translation (NAT) | Enables safety communication to a device addressed through NAT. |
Actual device address | Specifies the device's IP address on the Private Network of the NAT. It is the same
IP address found in the Internet Protocol view.This parameter is available when the Enable Network Address Translation
(NAT) checkbox is selected. |
Chassis size | Sets the chassis size of the rack that contains the adapter bridge device. Only the
valid chassis sizes are displayed. The chassis size cannot be set to a size that is less than the last device in the
chassis. This parameter is only available when the device is an adapter in the topology. |
Provide Feedback