By Gary Hida, Operations Manager, and Jason Santos, Operations Manager, Applied Control Engineering
An aging liquefied natural gas (LNG) plant is getting a complete makeover as a phased modernization that includes the installation of a modern distributed control system (DCS) that will, over time, replace the functionality of a legacy DCS. For more than 40 years, this plant has provided natural gas to the pipeline during periods of high demand in the winter. This upgrade is meant to provide the plant with a new lease on life.
The System as Found
The legacy DeltaV DCS in this facility had not been updated since sometime before 2010 and was operating on software that was not supported and computer systems that were out-of-date. The DCS was responsible for the tank controls and the boil-off gas (BOG) system with accommodations for hardwired communications to the Vaporizer and BOG compressor skids.
The hardwired communication to the skid-based equipment allowed for basic control and monitoring and was incapable of providing a full view of those systems to the supervisory control and data acquisition (SCADA) system. Documentation for the DeltaV control system also was lacking, and modifications to the process and automation systems were not tracked.
Furthermore, space in the plant was limited, and a modernization of this scope would require more than was available. To overcome this, the plant already had begun construction on a new motor control center (MCC), and a preliminary design for a new control room was already underway.
Phase 1: Install Modern DCS and Integrate New Vaporizer Skids
Three new vaporizers were installed as part of this phase, each with two Allen-Bradley® ControlLogix® programmable logic controllers (PLCs) for combustion control and burner management. A new PlantPAx® DCS from Rockwell Automation was developed with redundant process automation system servers (PASS) and two operator workstations (OWS).