Loading
Magazine | Process Safety
Recent ActivityRecent Activity

How Integrated SIS Can Boost Efficiency

Merging safety and process control onto a common platform, oil and gas OEMs can streamline workflows and offer users better uptime and safety.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Professional caucasian refinery worker in safety equipment checking gas pipeline installation and pressure.

By Liz Bahl Prosak, Commercial Portfolio Manager, and Kris Dornan, Marketing Manager for Large Controllers, Rockwell Automation

Equipment that’s built on a common automation architecture delivers benefits across its life span. By reducing the number of disparate technologies and interfaces, the equipment can be more quickly and easily developed, using fewer tools and less specialized knowledge. And it can simplify the jobs of everyone who interacts with it in a production environment.

Now, one more disparate technology can be folded into the automation architecture with the introduction of integrated safety instrumented systems (SISs).

Integrated SIS is built on the same platform as the base process control system (BPCS). This allows the two systems to be designed, implemented, operated and maintained together as part of a common architecture.

For OEMs, integrated SIS can simplify and accelerate projects that require process safety or hybrid process and machine safety. And it can help them better differentiate their equipment from the competition by giving users simplified systems, better insights and more efficient maintenance.

Decreased Engineering Time and Costs

For decades, the different control disciplines used in production environments — such as discrete, batch, process and motion — have been converging into a common integrated architecture. However, because the SIS historically has been built on a separate platform and used different logic, it has remained outside this architecture and operating in isolation.

By bringing the SIS onto the same platform as the BPCS, and thus into the common architecture, an integrated SIS simplifies how equipment is developed and deployed.

Keep up with oil, gas & chemical automation trends and technologies
oil rig in the Gulf of Mexico
Subscribe to The Journal
Keep up with oil, gas & chemical automation trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork’s digital magazine, and receive the oil, gas and chemical industry’s latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy!

Subscribe Now

Now, engineers don’t need to learn and use two different sets of tools for process and safety control. Instead, they can program and configure the SIS and BPCS together, using a common toolset and single knowledgebase.

The productivity-enhancing features in those toolsets — which until now could only be used on the common automation architecture — now also can be unleashed on the SIS.

For example, some design and configuration tools allow for multi-user collaboration, so engineers with different skillsets and in different locations can work on a project simultaneously.

In addition, some tools use disruptive technology such as AI to help answer engineers’ questions and troubleshoot errors. Extending these features to SIS programming and configuration can help engineers work more efficiently.

Additionally, developing a common human-machine interfact (HMI) display for safety and process control can be greatly eased in a common architecture. Engineers no longer need to map data from disparate systems that use different logic. Instead, they can use SIS and BPCS data that come from the same platform and are based on a common logic to more easily and intuitively create a display.

Integrated SIS solutions also can modernize how engineers approach process safety to deliver further time and cost savings in projects.

For example, traditional SIS solutions have required engineers to write custom add-on instructions to achieve SIL 2. But recently introduced integrated SIS solutions use the latest control and I/O technology and are engineered to achieve SIL 2 almost out of the box. Rather than writing custom code, engineers can now simply check some boxes for their safety configurations.

Engineers can also take advantage of modern control system capabilities available in integrated SIS solutions. Granular safety signatures, for example, compartmentalize safety functions to shorten SIS validation and testing times.

Production engineer with a laptop near process automation equipment in a chemical manufacturing plant.
Industry Perspective
Q&A: How Smart Devices are Transforming Process Instrumentation

In process automation, smart, connected instrumentation is key to improving productivity, lowering maintenance costs, complying with legal requirements and more.

To explore advancements in process instrumentation — including transmitters, sensors and actuators — and why they matter, The Journal From Rockwell Automation and Our PartnerNetwork's Executive Editor Theresa Houck spoke with Endress+Hauser’s Ashley David, Product Marketing Manager for Level and Pressure Equipment. Read their insightful interview.

Read the insightful interview (2-page PDF).

Read Now

Better Safety

An integrated SIS continues delivering value after equipment is handed off. It can simplify work for end users just like it can for engineers and reduce the total cost of ownership of their equipment.

Easing the jobs of production staff and helping them do more with technology is becoming more important as workforce challenges persist. According to the “NAM Manufacturers’ Outlook Survey, Third Quarter 2024”, 6 in 10 manufacturers say attracting and retaining a quality workforce is one of their biggest challenges.

Integrating the SIS and BPCS onto a common architecture allows operations and maintenance workers to learn and use just one set of hardware and software for both safety and process control.

Maintenance is streamlined, too. Now, spares are needed for just one common architecture instead of two disparate systems. And whether there’s an issue with the SIS or BPCS, technicians can work with just one vendor and don’t need to worry about finger pointing between vendors.

An integrated SIS can also help end users optimize productivity and uptime in their operations. For example, an SIS solution that’s engineered for high availability, while also offering advanced diagnostics and predictive maintenance capabilities, can minimize safety-related stoppages and other unplanned downtime.

The easier mapping of data from the SIS and BPCS into a common HMI could, for instance, give end users visibility into how close their process is to the point where the SIS needs to take over. This could allow them to intervene before issues cause shutdowns.

No More Barriers

The merging of safety and process control onto a common platform transforms process safety in a way that benefits the entire equipment life cycle. Now, OEMs can program, configure and commission equipment with SIS more easily, using more streamlined workflows and less specialized knowledge.

And they can offer customers equipment that’s easier to use and service, which can help them maintain both uptime and safety.

 

Like this article? Sign up for the digital magazine (4X/year) and e-newsletter from The Journal From Rockwell Automation and Our PartnerNetwork.

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

 

Topics: The Journal Safety Instrumented Systems Oil & Gas

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left The Journal
  5. Chevron LeftChevron Left How Integrated SIS Can Boost Efficiency