From Polytron
When the electrical technical engineer responsible for technical support and operations at a Fortune 100 consumer packaged goods (CPG) manufacturing distribution center learned that the variable-frequency drives (VFDs) installed across the entire distribution center soon would be obsolete, he knew he needed to act fast.
Unfortunately, the manufacturer’s distributed drives installed less than seven years prior were moving to the end of their life cycle in manufacture and support.
Because the manufacturer recently had implemented the large capital project to reconfigure its distribution center with more than 270 of the VFDs, the company was averse to another large capital outlay. However, the distribution center provides consumer products to most of its commercial and residential customers across the northeastern United States.
With no viable replacement from the supplier, the lead engineer was left to determine how he would find a long-term solution for replacing all VFDs.
The CPG manufacturer had a vested interest in continuing with the supplier’s products, so Polytron worked with the supplier and a local electrical supplier to design a distributed drive package that would be a feasible solution for the distribution center’s conveying network.