Loading
Magazine | Automotive Industry
Recent ActivityRecent Activity

How AMRs are Transforming Automotive Logistics

See how autonomous mobile robots are changing material handling for automotive tier suppliers, cutting costs and improving safety and productivity.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Silver automobile inner rear and front doors stacked on storage shelves.

By Renee Pieti, Auto Tier 1 Global Leader, Rockwell Automation

The competitive edge for tier suppliers in the automotive industry is razor-thin and shrinking fast. While the workforce shortage remains a priority as an ongoing, expensive constraint on growth, increasing global competition is also raising cost pressures. And while EV sales appear to be slowing, tier suppliers are still scrambling to meet demand as the powertrain evolution continues.

To help manage these challenges, tier suppliers are deploying autonomous mobile robots (AMRs) for material movement on the plant floor and between production, warehouse and shipping operations. AMRs help tier suppliers make significant advances in reducing costs, augmenting their workforce, optimizing production, and improving safety with indoor logistics.

Shift from Automated to Autonomous

An AMR can look like an Automated Guided Vehicle (AGV), but that’s where the resemblance ends. An AGV works like a conveyor, moving material from point A to point B. In contrast, an AMR functions more like a material handler, with the flexibility to move wherever the fleet manager sends it.

Some key ways AMRs allow tier suppliers to reduce costs and maximize productivity without compromising on safety include the following:

  • AGVs are preprogrammed, while AMRs have onboard intelligence to quickly choose faster, repeatable paths within the factory floor traffic rules. Onboard intelligence also lets AMRs navigate safely alongside people on foot or operating tuggers or other material handling equipment.
  • AGVs require physical infrastructure such as magnetic tape, wires and beacons to stay on track. AMRs don’t need this infrastructure to navigate the facility.
  • AGVs travel fixed paths in a controlled space; AMRs use machine learning (ML) to become more efficient and accurate as they encounter new situations throughout the plant floor.

As a result, the shift from automated to autonomous means AMRs often can more fully meet the demands of material-handler roles while lowering costs.

Main Image
Enjoy The Journal’s Automation Chat Podcast

Join Theresa Houck, Executive Editor of The Journal From Rockwell Automation and Our PartnerNetwork™ magazine, as she talks with industrial automation and manufacturing leaders, implementers and other subject matter experts on the magazine’s “Automation Chat” podcast. Learn about the newest technologies and trends affecting your job every day.

Listen on your favorite podcast app or on the web, or watch their conversations on YouTube. And subscribe so you don’t miss an episode.

Listen Now Watch Now

Material Handling Use Cases for AMRs

AMRs are transforming workflows as they move materials to and from people, floors, racks and stands, and between islands of automation. Some of the most effective use cases include moving materials along the production line (work in progress), automating lineside delivery, and automating the movement of nonconveyable materials.

Also, many facilities are using AMRs to replace manual or unsafe material handling processes.

As more AMRs enter the market, it becomes clear that not all AMRs play on the same field. Key differentiators include a design that maximizes uptime and options in payload capacity that let manufacturers closely align their AMR investment and capabilities with production needs.

Fleet management software is another distinctive advantage. Ideally, the software allows a single fleet manager to keep the facility’s AMRs moving safely and efficiently for increased throughput and uninterrupted operation.

Automotive parts production is a prime application for AMRs for tier suppliers of all sizes. FORVIA, the seventh-largest global automotive supplier, deployed eight AMRs from OTTO Motors by Rockwell Automation in its interior systems division for material movement between the work cell and the warehouse. FORVIA saw an 11-month return on investment and achieved a 15% reduction in work-cell size. The tier supplier is expanding its fleet by 50% after just 1.5 years of top results.

HIROTEC America, another global tier supplier, uses OTTO AMRs to complete production processes more reliably and consistently. Their ability to be up and running very quickly — even in a single day — without the need for infrastructure is helping HIROTEC move towards its goal of zero operators for spare parts production.

With global production growth projected to ramp up by 15% in the next four years, tier suppliers are deploying autonomous material handling solutions now to build capacity and operate at lower costs.

 

Like this article? Sign up for the digital magazine (4X/year) and e-newsletter from The Journal From Rockwell Automation and Our PartnerNetwork.

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

AMR in factory transporting materials
Learn About OTTO Motors

OTTO Motors by Rockwell Automation is quickly becoming one of the largest indoor logistics operators in the world. The company helps tier suppliers build their autonomous workforce with AMRs well-suited to their jobs in terms of payload capacity, travel speed and footprint. OTTO AMRs complete more than 400,000 monthly deliveries in production facilities, ranging from automotive to aerospace to consumer packaged goods.

OTTO helps fleet managers to use 20% fewer AMRs to accomplish the same or more than other AMR fleets. In addition, OTTO Fleet Manager integrates with a facility’s existing systems, streamlining handoffs in complex workflows with flexible APIs.

Learn More
Topics: The Journal Advanced Motion & Robotics Automotive & Tire
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left The Journal
  5. Chevron LeftChevron Left How AMRs are Transforming Automotive Logistics