Loading
Magazine | Water Wastewater
Recent ActivityRecent Activity

How AI Boosts Energy Efficiency in Wastewater Treatment

Using artificial intelligence to optimize energy-intensive aeration processes can cut energy consumption by 30-50% while improving process efficiency.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Overhead view of a wastewater treatment facility

By Lauren Harrington, Industry Director, North America Infrastructure, Rockwell Automation

In wastewater treatment, aeration plays a critical role in the fight against pollution and contamination and in the effort to protect communities and comply with new contamination regulatory requirements. This fundamental step of aeration is the cornerstone of wastewater treatment facilities worldwide.

It’s essential for purifying water by breaking down organic pollutants and ensuring its safety for reuse or discharge back into the environment. However, its voracious appetite for energy, accounting for 60% of facility power requirements, poses a considerable challenge to the operational costs and sustainability of wastewater treatment plants.

Role of Aeration

Aeration, simply put, is the process of infusing oxygen into wastewater to stimulate the growth of beneficial microorganisms. These microorganisms, in turn, devour organic matter to effectively cleanse the water of harmful pollutants such as pathogens, nitrogen compounds and organic chemicals.

Without adequate aeration, the microbial activity essential for wastewater treatment would grind to a halt, resulting in compromised water quality and environmental hazards.

The Energy Dilemma

Aeration is a crucial process, but it comes with a significant operational cost — energy consumption. Aeration systems use motors to continuously pump air into large basins that support the microbial population necessary for wastewater treatment. As a result, energy costs can account for up to 30% of a utility's total operation and maintenance (O&M) expenses, with aeration systems being the primary energy consumers within wastewater treatment plants.

Keep up with water wastewater industry trends and technologies
Main Image
Keep up with water wastewater industry trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork’s digital magazine, and receive the water wastewater industry’s latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy!

Subscribe Now

Due to the substantial energy demand of aeration systems, many wastewater facilities across North America are still obligated to inform their local power utility before activating these systems. The sudden surge in energy usage can strain the power grid, making advance notice necessary to prevent potential disruptions.

According to the International Energy Agency (IEA), the demand for energy in water wastewater utilities is expected to continue rising. This further emphasizes the need for efficient energy management and communication with power providers (see chart).

The Promise of AI

Artificial intelligence (AI) offers a promising solution to the challenges posed by energy-intensive aeration processes and the subsequent escalation of operational costs. AI's ability to analyze large amounts of data and make real-time adjustments has proven to be useful in optimizing aeration systems, reducing energy consumption by 30-50% while simultaneously improving process efficiency.

Here are a few ways AI optimizes aeration for energy efficiency:

Graphic from IEA showing demand for energy in water and wastewater utilities to continue rising

According to the International Energy Agency (IEA), the demand for energy in water and wastewater utilities is expected to continue rising.

  • Predictive Analytics. AI algorithms analyze historical data on wastewater flow rates, pollutant levels and weather patterns to predict optimal aeration requirements. By forecasting demand and adjusting aeration rates accordingly, AI minimizes energy waste and maximizes treatment effectiveness.
  • Dynamic Control Systems. AI-powered control systems continuously monitor and adjust aeration rates based on real-time conditions, optimizing energy use while maintaining treatment performance. These systems help ensure efficient operation while reducing energy consumption by dynamically responding to changes in effluent quality and flow.
  • Machine Learning Algorithms. Through machine learning algorithms, AI learns and adapts to the unique characteristics of each wastewater treatment plant. These algorithms achieve significant energy savings over time while improving treatment efficiency by continuously optimizing aeration parameters based on feedback loops.
  • Fault Detection and Diagnostics. AI-enabled analytics identify inefficiencies or malfunctions in aeration equipment, enabling proactive maintenance and minimizing energy losses due to equipment downtime or suboptimal performance.

Empowering Operators

AI's transformative potential in wastewater treatment extends beyond optimizing aeration for energy efficiency; it also serves as a powerful tool for empowering plant operators. By leveraging the real-time insights and predictive capabilities offered by AI, operators can make informed decisions, optimize resource allocation and ensure the plant performs at its best.

AI-driven automation can streamline processes and reduce the burden of manual tasks, freeing up operators to focus on higher-level strategic initiatives and problem-solving.

Beyond Energy Savings

Improving the aeration process in wastewater treatment is crucial, of course,l for removing conventional pollutants. But it also holds promise for addressing emerging contaminants like per- and polyfluoroalkyl substances (PFAS).

These “forever chemicals” — those that don’t break down easily in the environment and can persist for very long periods of time — are widely used in industrial and consumer products for their water- and grease-resistant properties. They have garnered increasing attention due to their persistence in the environment and potential health risks.

Solar panels with wind turbines against a mountain landscape against blue sky with clouds.
Podcast
How Digitization Helps the Renewable Energy Sector Meet Increased Demand from Manufacturers

In this episode of our “Automation Chat” podcast from The Journal From Rockwell Automation and Our PartnerNetwork magazine, Executive Editor Theresa Houck chats with Craig Blondin, Industry Sales Manager, Hybrid, at Rockwell Automation. Learn how renewable-energy technology manufacturers can scale up production quickly — without sacrificing product quality — to meet increasing demand from manufacturers awaiting these solutions.

These renewable-energy solutions will help manufacturers meet carbon-neutral and other sustainability goals while bolstering financial performance.

Listen on your favorite podcast app or on the web, or watch their conversation on YouTube.

** Named Best Podcast 3 Consecutive Years! 2022 - 2024 Apex Awards of Publication Excellence.

Listen Now Watch Now

With the first federal mandate recently signed to further restrict PFAS levels in water and wastewater, there is urgency to develop a plan for compliance. The importance of reducing, if not eliminating, these forever chemicals is unanimous; however, implementing solutions solely at the utility level is ambitious and costly.

An optimized aeration system could offer avenues for mitigating PFAS contamination through both direct and indirect mechanisms.

One direct pathway involves enhancing aerobic biodegradation, where microorganisms metabolize organic matter, including certain PFAS compounds, as a source of energy and carbon. By optimizing aeration conditions such as dissolved oxygen levels, temperature and pH, wastewater treatment plants can promote the growth and activity of microbial consortia capable of breaking down PFAS molecules. This isn’t proven for all PFAS species, but has worked well for some. 

Indirectly, aeration can serve as a pretreatment step by introducing oxygen into the water matrix and promoting the formation of reactive species through mechanisms such as ozonation or photolysis. Consequently, subsequent treatment stages can benefit from the presence of these oxidants, accelerating the degradation of PFAS and improving overall treatment efficiency.

Using AI to optimize aeration in wastewater treatment can contribute to broader strategies aimed at reducing PFAS inputs into the environment. By enhancing the removal efficiency of treatment processes, fewer PFAS compounds are discharged into receiving water bodies, minimizing the risk of contamination and ecosystem exposure.

However, continued research and innovation are essential to refining these strategies and ensuring their efficacy in diverse wastewater treatment contexts.

Pioneering a Sustainable Future

The integration of AI into critical wastewater treatment processes represents a transformative step in the journey toward a more sustainable future. By using AI to optimize aeration for energy efficiency and enhanced performance, wastewater treatment plants can achieve significant cost savings and reduce their environmental footprint.

In addition, AI-optimized aeration systems may offer new avenues for mitigating the impact of persistent pollutants such as PFAS, and thus contribute to a more comprehensive approach to water-quality management. As we continue to innovate and refine these technologies, the integration of AI in wastewater treatment holds promise for ensuring the provision of clean, safe water for reuse and discharge.

 

 

Like this article? Sign up for the digital magazine (4X/year) and e-newsletter from The Journal From Rockwell Automation and Our PartnerNetwork.

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

Topics: The Journal Water Wastewater

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left The Journal
  5. Chevron LeftChevron Left How AI Boosts Energy Efficiency in Wastewater Treatment
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose