Loading
Magazine | Oil & Gas
Recent ActivityRecent Activity

Energy Firm Turns Oilfield Gas Flares Into Income

An energy services provider applied an Integrated Architecture that delivered a gas-conditioning plant in 9 months and captures $200,000/day in revenue.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Grupo Nuvoil Ascend automation natural gas flaring site.

Whenever crude oil is extracted, water, sand and natural gas are part of the mixture. And when large reserves were discovered in the Ixachi field south of Veracruz, Mexico, extracting and transporting the oil was the relatively easy part. Separating and shipping the oil via pipeline is always straightforward. Managing the natural gas is another matter.

“Oil is handled like a liquid and transported by pipeline or truck,” says Mudar Jamal Eddin, engineering director, Grupo Nuvoil. “Natural gas must be processed and compressed before it can be transported in commercial pipelines.”

If a processing plant isn’t accessible, producers typically ignite or “flare” the natural gas to dispose of it. This practice is wasteful and raises environmental concerns. Flaring also represents a lost source of revenue for oilfield operators. Therefore, Ixachi needed to make the most of scarce resources.

To keep flaring to a minimum and maximize returns, Ixachi operators asked Nuvoil to deliver a gas-conditioning plant near the oilfield as quickly as possible. Nuvoil is a major energy services and solutions provider headquartered in Veracruz.

Compressed Schedule, Complex Process 

The scope of work for the gas-conditioning plant included engineering, procurement and construction — and operation and maintenance of the completed plant. Located on 32 acres about 10 miles from the well pad, the completed Papan Gas Processing Plant was specified to process 345 million standard cubic feet (345 MMSCFD) of natural gas per day.

“While the timeline was challenging, we knew we had the capacity to meet our customer’s needs,” Eddin says. “We had built similar plants in the past — and flare avoidance is our core business.”

To meet customer requirements, Nuvoil designed a cryogenic gas processing system. The complexity of the system is difficult to overstate.

Keep up with oil, gas & chemical automation trends and technologies
oil rig in the Gulf of Mexico
Subscribe to The Journal
Keep up with oil, gas & chemical automation trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork’s digital magazine, and receive the oil, gas and chemical industry’s latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy!

Subscribe Now

At the wellhead, oil, water, sand and natural gas are separated. The resulting “sour gas,” which contains sulfur, enters the Papan Gas Processing Plant at about 200°F. In the first step, the gas is chilled to 120°F and residual sand and dirt are separated.

Next, the gas enters the sweetening plant, where sulfur is removed — and then moves to a molecular sieve dehydration system, where humidity is absorbed. In the subsequent chilling process, the gas temperature drops to about -121°F.

“Chilling triggers gas condensation,” Eddin explains. “As a result, we can remove LPG (propane/butanes) and other hydrocarbons. What remains is almost pure methane and ethane.”

Finally, the gas is compressed for transport via commercial pipelines.

Managing 3,000+ Data Points

To speed implementation of the plant, Nuvoil chose a control system integrator they had successfully worked with in the past, Ascend Automation & Controls, a Bronze OEM Partner in the Rockwell Automation PartnerNework™ program. Ascend is a division of CAM Integrated Solutions.

“Our company is very familiar with gas conditioning systems,” says Horacio Tinoco, vice president, Ascend Automation & Controls. “We developed a control system for Nuvoil about 11 years ago. Of course, the new system enables even more sophisticated and efficient operation.”

The Rockwell Automation control platform is based on Allen‑Bradley® ControlLogix® process controllers and a FactoryTalk® View HMI. To ease system monitoring, Nuvoil relies on a video wall in the plant featuring twelve 55-in. displays and four operator workstations in the control room.

To manage the process, more than 3,000 instruments are physically connected to the system – and nearly 150 PID loops are included.

“In a complex system like this, the data points multiply rapidly,” says Tinoco. “Using data trending, Nuvoil can produce reports to support operations, maintenance or custody transfer.”

In addition, Ascend will be adding  software to the system soon.

An oil drill in a field at sunset.
eBook
2023 Oil & Gas Automation

In the "2023 Oil & Gas Automation" eHandbook, learn how to optimize gas pipeline & facility throughput, and how pressure affects Coriolis flowmeters. Also see how an ethanol producer increased capacity by 12%, a major petroleum firm increased production by 548 BOPD, and a ground-breaking biogas hydrogen sulfide removal system cuts chemical use and waste.

And learn about leading-edge Universal Industrial Gateway technology and a new valve manifold with Industry 4.0 automation.

Published by The Journal From Rockwell Automation and Our PartnerNetwork™ magazine.

Download Now

“First, we focused on getting the plant up and running,” Tinoco explains. “Now, we are aiming to provide long-term data storage capabilities so Nuvoil can run analytics for multiple purposes.”

Exceeded Expectations

Nuvoil completed the plant in 9 months and was running at full capacity within 12.4 months. Today, the plant processes about 320,000 cubic feet of gas daily, representing revenue of about US$200,000 each day.

“When oilfield operators flare gas, they are burning resources — and burning money,” Tinoco says. “Gas conditioning facilities open up an additional source of revenue.”

Ascend plans to partner with Nuvoil as they continue to optimize plant operations.

“Currently, we are exploring artificial intelligence (AI) options to enhance efficiency,” says Eddin. “We are evaluating our exact needs so we can match it with the products that Rockwell Automation offers — and add those capabilities.”

 

Like this article? Sign up for the digital magazine of The Journal From Rockwell Automation and Our PartnerNetwork and get articles like this delivered right to your inbox.

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

Topics: The Journal Smart Manufacturing Digital Transformation Oil & Gas Graphic Terminals Programmable Controllers
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left The Journal
  5. Chevron LeftChevron Left Energy Firm Turns Oilfield Gas Flares Into Income