Loading
Magazine | Food and Beverage
Recent ActivityRecent Activity

Dairy Farm Cuts Chemical Use by 50%

A standardized control system helps a 30,000-head dairy farm simplify its complex milking operation, lower maintenance and meet sustainability goals.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Brown Jersey cow mother and calf grazing in a grassy field.

For Bill and Susie Millenkamp, success in agribusiness is built on a passion for optimal animal care, cleanliness, strict protocols, staff training and technology. What began as a calf ranch in the mid-1990s has grown into Millenkamp Cattle, Inc., a vertically integrated business that encompasses the ranch, farm, feedlot, cow-calf operation, and the Idaho Jersey Girls Dairy, a large-scale milking operation.

“At any given time, there are about 36,000 calves at the Jerome, Idaho operation, and at the Idaho Jersey Girls Dairy they are milking approximately 30,000 cows,” says Mark Harrison, operations manager at Millenkamp Cattle, Inc.

Milking in the 21st Century

As milking operations ramped up in 2015 with the completion of Milk Barn #1, the Millenkamps called on local system integrator, Automation Werx, for network, communication and technology support. Automation Werx is part of the Rockwell Automation System Integrator PartnerNetwork™.

Milk Barn #1 features two 106-stall rotary milking parlors designed to harvest milk from about 15,000 cows. Each parlor features three robots that provide pre-milking sanitizing, udder stimulation and post-milking teat sanitizing.

The milking operation also includes ventilation, pumping, chilling and clean-in-place (CIP) systems, as well as solutions that offload the milk to tanker trucks. 

“There was a lot of stand-alone, third-party equipment in Barn #1,” says Trevor Steffler, co-owner of Automation Werx. “Our goal was to provide the dairy with an integrated system that would enable their team to monitor equipment from a centralized location.”

To meet objectives, the system integrator delivered a networked supervisory control and data acquisition (SCADA) solution featuring FactoryTalk® View Supervisory Edition (SE) HMI software from Rockwell Automation. 

Keep up with food & beverage automation trends and technologies
workers in a cookie food manufacturing plant
Subscribe to The Journal
Keep up with food & beverage automation trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork™, and receive the latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy to keep up with updates in the food and beverage industry!

Subscribe

When the dairy owners planned to more than double its milking operation five years later, the Millenkamps again asked Automation Werx for a solution.

Integrating Disparate Equipment

For Milk Barn #2, Idaho Jersey Girls installed four 106-stall rotary parlors, with associated robotics and auxiliary systems. Automation Werx was tasked to work with multiple vendors and deliver a state-of-the-art system that would largely replace third-party controls with a unified Rockwell Automation platform. A critical project objective was to minimize downtime.

“We are milking 22 hours a day and are down one hour for equipment sanitizing,” Harrison says. “In addition, cattle are creatures of habit and require a consistent milking schedule. We can’t afford downtime.”

The system integrator designed an integrated solution built on a PlantPAx® distributed control system (DCS). The solution features Allen-Bradley® programmable controllers, PowerFlex® AC drives, Stratix® Ethernet managed switches and FactoryTalk View SE.

“We’ve added multiple levels of redundancy at various points in the system,” explains Nick Reichelt, co-owner, Automation Werx. “For example, we used seven drives on each carousel, although only five are required, so there’s no interruption for drive maintenance.”

Most important, PlantPAx DCS delivers data, analytics and insights through easy-to-understand dashboards that help workers quickly respond to abnormal situations like alarm logs and unexpected downtime events.

Keeping It Sustainable

Automation Werx also aligned control system capabilities with the dairy’s sustainability goals.

“We’re farming over 14,000 acres for feed and compost all our manure for fertilizer,” Harrison notes. “And this is probably the cleanest dairy you’ll ever see. We take great pride in that.”

Idaho Jersey Girls Dairy also is focused on reducing its use of chemicals to clean and sanitize equipment. Chemicals have an environmental impact and also represent the single largest cost to the dairy. The Automation Werx solution manages all chemical batching, from udder sanitation and cattle foot baths to the CIP system.

“The CIP system includes conductivity sensors to measure the level of chemicals in the cleaning solution,” explains Reichelt. “To save on chemicals, the system captures the final rinse in the first batch and reuses it for the first wash of the next batch.”

Water used in the chillers is also recaptured and reused for floor flushing and other cleaning tasks.

The dairy estimates that CIP cleaning solution recapture decreased chemical usage by more than 50%, when compared to a conventional barn. And because the batch solution maintains a constant water and chemical temperature, CIP cycle time was reduced by about 30 minutes.

Simplified Operations

“When we started to move toward automation, we thought we were going to have to learn 10 different control systems to manage all equipment,” Harrison says. “But with the new system, we can monitor everything from a central location and see exactly where a downtime event has occurred.”

“The troubleshooting time you save? I can’t even put a number on that — it’s huge.”

Automation Werx continues its work with Idaho Jersey Girls Dairy, focusing on future enhancements that align with the operation’s vision.

“Our goal is to migrate Barn #1 to the PlantPAx system,” Steffler says. “Ultimately, we plan to build a unified system incorporating both barns — all controlled and monitored from one central location.”

 

Like this article? Sign up for the digital magazine (8x/year) of The Journal From Rockwell Automation and Our PartnerNetwork and get articles like this delivered right to your inbox.

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

Theresa Houck, Executive Editor, The Journal From Rockwell Automation and Our PartnerNetwork magazine
Podcast
9 Industrial Automation Trends in 2023

In this episode of The Journal’s award-winning Automation Chat podcast, “9 Industrial Automation Trends in 2023,” Executive Editor Theresa Houck discusses important trends helping manufacturers and producers with digital transformation and the skilled worker shortage.

Learn about smart technologies and strategies, including no-code automation, 5G, additive manufacturing, Artificial Intelligence, virtual reality (VR), augmented reality (AR), robotics, blockchain, wearables and more.

Listen on your favorite podcast app or on the web.

Listen Now
Topics: The Journal Food & Beverage FactoryTalk View SE PlantPAx Programmable Controllers Drives
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left The Journal
  5. Chevron LeftChevron Left Dairy Farm Cuts Chemical Use by 50%