By Matt Weaver, Global Technical Director and Chief Enterprise Architect at Rockwell Automation
The life sciences industry operates under immense pressure to maintain product quality, meet strict regulatory standards and optimize efficiency. Many manufacturers struggle with outdated systems and processes that slow production and increase the risk of noncompliance.
As of late 2024, only 31% of life sciences compliance and risk leaders felt “very prepared” to meet compliance and risk challenges, with 56% expecting to face more resource constraints.
Wearable devices and biometric technology offer to ease these burdens, improving compliance, accelerating workflows and supporting employee productivity. Here are eight ways these technologies are transforming operations across the industry — and what manufacturers need to know to adopt them effectively.
1. Reduce Compliance Burdens Through Automation
Regulatory compliance is the backbone of life sciences manufacturing, but it’s also a major time commitment. Every step of the process needs to be documented, verified and audit ready.
Traditionally, this has meant a lot of paperwork, passwords and manual checks. It’s tedious and prone to errors. Wearables and biometric technologies offer a way to automate and simplify compliance while maintaining the high standards regulators demand.
2. Strengthen Security with Biometric Access Control
Biometrics such as fingerprint or facial recognition offer a more secure and reliable method for granting access to sensitive workflows and systems. Unlike passwords or swipe cards, which can be shared or stolen, biometric credentials are unique to each individual, making them harder to compromise.
These technologies also generate detailed, auditable logs that track who accessed specific areas or systems and when. This is particularly useful during inspections or audits, as manufacturers can quickly demonstrate adherence to access control protocols without poring over manual records.
3. Monitor Protocol Adherence in Real Time
Wearables like smart badges or wristbands equipped with proximity sensors and motion trackers can monitor whether employees are adhering to critical protocols. These logs can create an audit trail, reducing manual checks and human error, making it easier and faster for manufacturers to stay compliant and secure.
4. Eliminate Bottlenecks in Critical Workflows
Efficiency is critical in life sciences manufacturing, where delays can impact supply chains and, ultimately, patient outcomes. Yet bottlenecks persist. Wearables and biometrics help manufacturers eliminate these obstacles, shaving time off critical processes without compromising quality or safety.