Company to showcase methods for achieving higher levels of reliability while reducing operational costs
MILWAUKEE — Rockwell Automation will feature a suite of solutions for the power generation industry to enhance efficiency, optimize plant operations and meet regulatory requirements at POWER-GEN International from Dec. 13 to 15 in Orlando, Florida.
At the Rockwell Automation booth (4236), industry professionals can learn more about integrated plantwide control systems, specifically focused on the PlantPAx distributed control system, which provides seamless integration between critical process areas and the balance of the plant. This enhanced visibility to real-time production information from the turbine to the transformer helps enable faster, more reliable decision-making.
“Today’s energy producers are looking for ways to maximize existing assets to increase power generation reliability and availability. An integrated control system can help to optimize and measure productivity, access and analyze critical process data, and help to reduce
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Kristen Crump
Rockwell Automation
414.544.2076
klcrump@ra.rockwell.com
Alyssa Samson
PadillaCRT
612.455.1914
alyssa.samson@padillacrt.com
PlantPAx is a trademark of Rockwell Automation Inc.
Published November 28, 2016