CIP Security protects critical communications in a Connected Enterprise
PHILADELPHIA — As industrial companies use digital transformation to improve productivity and profitability, they must also address its inherent security risks. CIP Security was created to help protect critical industrial communications as part of a defense-in-depth security strategy. Now, Rockwell Automation is introducing the first industrial control products on the market that allow companies to deploy CIP Security in their operations.
ODVA, a global association of the world’s leading automation companies, developed CIP Security. It is an extension to the Common Industrial Protocol (CIP), which is the application-layer protocol for EtherNet/IP. CIP Security is the first industrial automation protocol to support transport layer security (TLS), the most proven security standard in widespread use on the World Wide Web today.
“CIP Security can protect devices and systems that use EtherNet/IP from some of the top risks in connected operations, such as unauthorized PCs,” said Tony Baker, portfolio manager, security, for Rockwell Automation. “It does this in a few key ways. First, it limits device connectivity to only trusted PCs and devices. It also guards against packet tampering to protect data integrity. Finally, it encrypts communications to avert unwanted data reading and disclosure.”
Engineers will be able to implement CIP Security in their systems through new Rockwell Automation products and firmware updates to existing products such as Allen-Bradley ControlLogix controllers, communication modules and Kinetix servo drives.
In addition, the newly enhanced FactoryTalk Linx communications software allows FactoryTalk visualization and information software running on a PC to communicate to CIP Security-enabled devices. The new FactoryTalk Policy Manager tool within the FactoryTalk software suite is used to implement and configure security policies between CIP Security-enabled devices.
Rockwell Automation developed this new capability to work with existing industrial control devices regardless of whether or not they were designed to support CIP Security. This allows industrial users to phase in security over time and retrofit existing installations.
In addition, Allen-Bradley ControlLogix 5580 controllers will soon be certified compliant with the IEC 62443-4-2 security standard, building on the IEC 62443-4-1 certification that the Rockwell Automation Security Development Lifecycle has already received.
This latest certification means the controllers will meet the global standard’s robust cybersecurity requirements to help companies secure their connected operations. The ControlLogix 5580 family of controllers is one of the first platforms on the market to achieve this compliance.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 23,000 people serving customers in more than 80 countries.
Media Contacts
Steve Ludwig
Rockwell Automation
440.646.4013
swludwig@ra.rockwell.com
Leanne Hanson
Padilla
612.455.1776
leanne.hanson@padillaco.com
Allen-Bradley ControlLogix, FactoryTalk and Kinetix are trademarks of Rockwell Automation Inc.
Common Industrial Protocol, CIP Security and EtherNet/IP are trademarks of ODVA.
Published November 15, 2018