Rockwell Automation’s Milwaukee headquarters is the latest stop of the National Association of Manufacturers’ and The Manufacturing Institute’s “Creators Wanted” tour on Thursday, May 13.
The event, titled “Spotlight on the Future of Work,” will feature representatives from Rockwell Automation and the MI to explore advancements in smart manufacturing and preparing the workforce of tomorrow. This one-hour roundtable discussion will include comments from Rockwell Automation Chairman and CEO, Blake Moret, and a live question/answer session with industry experts on the skills and experience needed for a modern manufacturing career. It will also showcase Rockwell’s Academy of Advanced Manufacturing program, which has graduated and placed more than 225 U.S. military veterans in advanced manufacturing jobs.
To register to attend this free event, click here. For more information on Creators Wanted, visit live.creatorswanted.org.
Published May 12, 2021