Rockwell Automation has released a new line of IEC industrial relays that save energy and simplify selection.
Click to download image.
The new Allen-Bradley Bulletin 700-EF control relays offer universal wide-range coils. Four coil options cover control voltages from 24V to 500V, 50 to 60 Hz DC, making selection easier. These contactors save energy by reducing inrush apparent power (VA) by up to 68% and sealed VA by over 75% compared to standard, non-electronic coils and allow coil input terminals to be moved from the line to load side of the contactors without disassembly.
The Bulletin 700-EF relays are ideal for applications that involve switching heavier loads in industrial environments.
Allen Bradley and Rockwell Automation are trademarks of Rockwell Automation Inc. Trademarks not belonging to Rockwell Automation are property of their respective companies.
Published February 18, 2021