Loading

Recent ActivityRecent Activity

Data Analytics Help Boost OEE at Rockline Industries

Challenge

  • With cumbersome manual data-collection system, the company lacked real-time insight into specific information on machine production, performance and activities

Solutions

  • Data Analytics Solution - FactoryTalk Metrics software monitors plant-floor equipment, providing accurate, timely, granular and specific information on machine production, performance and activities.
  • System Design and Delivery - Stone Technologies, a Rockwell Automation Information Solution Partner, designs and delivers solution based on FactoryTalk Metrics software

Results

  • Increased OEE and Throughput - Each of five manufacturing cells have demonstrated an OEE increase of more than 20 percent compared to the prior system implementation.

Americans are more germ-conscious than ever. That’s one factor fueling the demand for hard-surface disinfectant wipes, which are designed to remove bacteria and viruses on everything from kitchen counters to doorknobs.

Convenience is another major factor: You can simply pull the ready-to-use wipes from a plastic canister, rather than turning to the more traditional spray-and-paper-towel method of household cleaning.

Rockline Industries has built a healthy business by manufacturing these disposable, private label wipes for major retailers. At its plant in Sheboygan, Wisconsin — one of seven the company operates globally — Rockline produces millions of wet-wipe canisters a week.

“It's been a great run for these product lines and the demand continues to skyrocket,” said Pat Rusch, operations manager at Rockline’s Sheboygan plant, which also manufactures coffee filters. “We can sell every canister we can produce.”

At the same time, he said, “It's been a tremendous challenge scaling our operations with that growth.”

That means that any increase in incremental capacity is well worth the return in revenue.

“An incremental 5 percent in throughput is an incremental 5 percent in capacity for us, which means an incremental 5 percent that we can sell,” explained Frank Hacker, general manager at the plant.”

To capture those dollars, plant management embarked on a journey in 2006 to obtain the real-time data that’s essential to drive continuous improvement.

A Backward System

Back in 2006, the overall equipment effectiveness (OEE) for many of the manufacturing cells on the wet-wipe side of the plant was below 50 percent.

Improving that number would require better visibility into how the lines and the individual machines were operating within in the five large work cells, which operate 24 hours a day.

Each manufacturing cell is dedicated to producing a specific size or type of wet wipe. The products vary in count and ingredients, including different sanitizing formulations and scents.

The high-speed packaging process begins with a “parent” roll of nonwoven fabric or substrate, which is automatically slit, perforated and wound into individual rolls of wipes. The rolls then are placed into rigid plastic canisters and filled with liquid ingredients. The container lids go on next, then the labels. Finally, the canisters are packed in trays or cases, and palletized for distribution.

Each manufacturing cell contains a series of machines and equipment that are strung together in series. Maintaining the right balance and speed on the line is critical to avoid common bottlenecks, like a jams in a capper, labeler or filler, that disrupt the flow and trigger unplanned downtime

Before 2006, each of these events would be captured manually. Whenever a machine went down or came back up, an operator would enter the time on a piece of paper, as well as line speeds and other parameters. Later, technicians had to key the handwritten metrics into an Excel spreadsheet, which was then shared with operators, managers and engineers in various plant departments.

“Our paper-based system for production reporting was very cumbersome when it came to trying to understand and analyze data,” said Hacker. Another problem: The system only looked backward. “We needed to understand our assets in real time. With that information, we could also look forward to see how we could fine-tune the process to increase throughput and reduce costs.”

Rusch added, “It became very obvious that the only way to sustain growth was to find a tool or a set of tools that would allow us to consistently deliver year on year continuous improvement.

Up-to-Speed Solution

In search of a solution, the Sheboygan plant managers turned to Rockwell Automation and Stone Technologies. Allen-Bradley products already were the cornerstone of the plant’s manufacturing infrastructure.

Managers consulted with Rockwell Automation experts in their local distributor’s office, as well as during the annual Automation Fair® event, which showcases the most advanced manufacturing hardware, software and integrated solutions from Rockwell Automation.

Rockline managers were impressed by the capabilities of the company’s FactoryTalk® Metrics software as a potential solution for monitoring its plant-floor equipment. The solution helps provide accurate, timely, granular and specific information on machine production, performance and activities.

“Given that we were already using an Allen-Bradley control system, FactoryTalk Metrics was the ideal option as it would integrate seamlessly to the technology we already in place,” Hacker said.

To convert that option into reality, Rockline put together a team consisting of its own engineering experts, some from Rockwell Automation and others from Stone Technologies, a Rockwell Automation Information Solution Partner. They approached the project in systematic stages, starting with one cell and a scaled-down version of the software solution – meaning it collected a limited selection of data.

The results of the pilot far exceeded Rockline’s expectations. Managers had projected a six-month pay back on initial project, but got their return on investment in three months.

“Within a couple of weeks of implementing the FactoryTalk Metrics solution, we saw an immediate 5 percent gain in OEE and throughput,” Hacker recalled. “That was enough to see the system was well worth the benefits. Just by being able to react and to respond to issues in real time, we were minimizing downtime and optimizing uptime.”

As Dan Engelhard, a director at Stone Technologies, explained, “Previously, Rockline was catching big downtimes, but missing the micro stops. With the Rockwell Automation data analytics solution, Rockline could now understand those stops and how they were disrupting continuous flow.

The results justified moving the FactoryTalk software into the other manufacturing cells. By that time, employees in others cells were clamoring for the new system.

Each cell underwent a “hard” transition, meaning the software replaced the manual data-collection system virtually overnight. To quickly bring operators up-to-speed on the computerized solution, training experts from Stone Technologies knew they needed to take an immersive approach.

“Cultural adoption of a new system can take a while in many companies,” Englehard said. “Rockline, with our assistance, became very aggressive in that arena. Operators weren’t allowed to use pencil, paper or clipboards after the system went live. We went straight to the screens."

Employees can view the real-time status of the operation from any vantage point in the cell. Large panel displays in the center of each work center scroll data points at a steady rate. During downtime – scheduled or unplanned – the displays become giant clocks that track the time required to return to normal operations.

“Seeing the numbers from the FactoryTalk solution motivates our operating teams and helps drive accountability,” Hacker said.

The intuitive nature of the system also eased the transition.

“From an operator perspective, FactoryTalk Metrics are easy to read, easy to interface with, and easy to get information out of,” Rusch said. “From engineering-management perspective, the data is instantly credible and critical for charting continuous improvement.”

Rockline improvement teams have used the data to understand the crux of problems on the line. For instance, the capper in one of the cells was showing a significant amount of intermittent downtime, triggering stops on the line. By analyzing production data, engineers identified the raw material (lid) as the root cause.

“We went to Stone Technologies and Rockwell Automation for help to cure our raw material issue,” Hacker said. “Data delivered from the solution showed the impact of the material on our process. We couldn’t do that before.”

World-Class OEE

Today, OEE in each manufacturing cell exceeds 70 percent.

“We went from mediocre to world-class,” Hacker said. “That never would have happened without the Stone Technologies solution based on FactoryTalk software.”

Canister production in each cell improved; Rockline saw the biggest increase on its cell with the highest demand, which increased output by over 180,000 units a week.

“FactoryTalk Metrics allowed us to take advantage of all incremental capacity,” Hacker said. “Quality is also up because line operators can react to problems sooner.

Rockline’s improvement teams are focusing on their next project using FactoryTalk data:  reducing waste and scrap. They are also using Stone generated information as an input for process simulation and modeling.

By using live data, they can evaluate the impact of process changes or equipment upgrades on overall performance. This allows them to identify key opportunities and maximize future capital investment.

“The system will do the heavy lifting for us,” Hacker said. “And we expect similar results.”

The results mentioned above are specific to Rockline Industries’ use of Rockwell Automation products and services in conjunction with other products. Specific results may vary for other customers.

Trademark Information: FactoryTalk Metrics is a trademark of Rockwell Automation Inc.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.